10/25/2020 6:05 AM | |
Joined: 6/5/2016 Last visit: 3/27/2024 Posts: 2 Rating: (0) |
Dear, We have PCS7 Version 6.2 with WINCC V6.2 SCADA system for substation. The WINCC is now working in Windows XP workstation. We planned to upgrade windows XP to Windows 10. Since Windows 10 not support WINCC version 6.2 we migrated the project to WINCC 7. But after migration the project started but in some graphic page it is showing UNKNOWN OBJECT. Kindly can you support in this issue. During migration there was no error. Also i doubt may be it is due to any special script used to make the graphic for circuit breaker open and close status. Kindly can you guide us to do proper migration without any error. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 10/26/2020 10:50:32New subject after splitting |
|
10/26/2020 10:51 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating: (172) |
Closed cause question posted twice. The second thread with the subject Migration from WinCC 6.2 to WinCC 7 error is published within the conference SIMATIC WinCC. Best regards, |
Follow us on