1/16/2018 6:01 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating:
|
Hello, Please check if you have set related parameters correctly. P2604 = start direction of searching cam P2605 = speed for searching cam P2606 = Maximum distance for searching of cam P2608 = speed for searching zero mark p2609 = Maximum distance for searching zero mark p2611 = Speed for searching reference point. Most important signal CWL & CCWL should not be high. Please refer attached sheet about the signal sequence to understand external cam signal referencing better. HTH AttachmentV 90 External cam referencing signals.pdf (301 Downloads) |
This contribution was helpful to
1 thankful Users |
10/29/2020 7:55 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating:
|
New question published by AutoGen_5218103 is split to a separate thread with the subject F7491 and F7492, EPOS stop cam reached.. Best regards |
Follow us on