10/29/2020 6:20 PM | |
Joined: 11/8/2017 Last visit: 7/12/2024 Posts: 328 Rating: (180)
|
Hi, I'm assuming you've seen the attached PDF? My understanding is that CC V4 has only been tested by (and approved by) Siemens to run on VSphere 6.0, 6.5 and 6.7. Depending on the complexity of your setup (i.e. it's a simple server on it's own; it's a distributed system; or if you have multiple servers for redundancy purposes) it may be the case that in some instances CC V4 will run fine on VSphere 5.5 - but it's unlikely to have been tested and approved by Siemens, and certain functions may not be available with 5.5. This may prevent you from getting any assistance from Siemens if there are issues with your system. Come back to us if you have any further questions. For now though, my advice is that you should approach your local Technical Support people who can advise you further. Regards, AttachmentGMS_Technical_Note_-_DesigoCC_v4.0_VMWare_VSphere_a.pdf (337 Downloads) |
This contribution was helpful to1 thankful Users |
Follow us on