6/18/2019 12:54 PM | |
Posts: 25 Rating: (0) |
We are currently testing out the Long Term Archive example, but are facing some issues related to the restore log procedure for the panel version in the example. It seems to archive logs successfully, but when we are trying to restore archived logs it fails and returns with following system events: 80053: Error during read access to closed log %1 80035: Initialization error, backup generation and reset failed. 80015: RestoredLog0 - is corrupted 80029: Log initialization ended. %1 logs reported errors. We have tested the PC runtime with simulator and this is running without any issues. Some specs: Tia V15.1, TP1500 Comfort (6AV2-124-OQC02-0AX0) |
Last edited by: flubber at: 06/18/2019 13:14:50Last edited by: flubber at: 06/18/2019 13:23:19Last edited by: Jen_Moderator at: 06/19/2019 08:49:59Optimized link. |
|
5/7/2020 5:09 AM | |
Joined: 8/16/2019 Last visit: 3/18/2024 Posts: 4 Rating: (0) |
Hi flubber, How are you, I am also facing same issue like you. Please advise you have fixed issue if yes how you have fixed can you share information possible. Please note I get issue when I try to restore archive log and then after this system also stops logging. I am using following 1. Tia v16 2. TP700 comfort. 3. I am storing current log and Archive log in USB. Regards
|
Follow us on