Industry Online Support
Technical Forum
1/21/2009 9:00 PM | |
Posts: 2661 Rating:
|
Hi xiaoxiaowu21,The minimum scan time of 100 ms is required because calling all blocks in OB1 makes the OB1 cycle time uneven and hence unstable. It is possible to have a scan time of more than 100ms. In that case the minimum should be adjusted accordingly. See attachment. Which version? Regards AttachmentCEMAT_MinScanTime.pdf (155 Downloads) |
Follow us on