11/3/2020 6:35 PM | |
Posts: 7 Rating: (0) |
@Fe_lipe are you suggesting that the only way to make it work is to downgrade the image? There's been quite a few changes since the image you suggested to downgrade to. We would appreciate if it was possible to fix the problem from the current version of the image... We've already spent so much time on this (there is a separate thread here: https://support.industry.siemens.com/tf/ww/en/posts/how-is-it-possible-to-diagnose-whether-the-communication-to-the-sim-card-works-well/240858/?page=0&pageSize=10 ), it is quite not professional to be honest. For so long we have tried to debug this problem thinking it was something we did not do well but it was not actually re-tested on your side, there was no acknowledgment of a problem. The gateway is advertised to be working with a 3G modem. But digging more into it, it is working only on a past image of the gateway. So basically we need to choose, do we want the latest gateway features or a 3g connection? On our side, we have made quite significant work to create a custom image catered to our needs based on 2.2.6. So what should we do to get a 3g connection? ------------------------------------------------------------------------------------------ |
Last edited by: opichon at: 11/03/2020 18:40:55Last edited by: opichon at: 11/03/2020 18:42:04Last edited by: opichon at: 11/03/2020 18:43:29Last edited by: opichon at: 11/03/2020 18:51:25Last edited by: Jen_Moderator at: 11/04/2020 09:16:51New subject after splitting |
|
11/5/2020 8:33 AM | |
Posts: 7 Rating: (0) |
Thanks, yes that's what we had to do in the meantime. Looking forward to hearing from you if you get the chance to fix this. Thanks |
Follow us on