11/5/2020 11:45 AM | |
Joined: 3/14/2008 Last visit: 10/14/2024 Posts: 2110 Rating: (942)
|
Hi, Thank you for the feedback. It is appreciated. That is the main advantage of a master library. You can retrieve the library on multiple projects and all are working with the same master library. You can get however problems. For example, when a block is updated to a new version which is used inside a CMT or PTT, and you copy that CMT/PTT to another project, you will need to update the new block version in that project as well. |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on