5/22/2018 11:33 PM | |
Joined: 6/14/2016 Last visit: 9/19/2022 Posts: 2 Rating: (0) |
I have a problem connecting to SIPROTEC 7SJ621 via the front interface RS232. When i try to connect i choose to work with device data and it starts downloading. After a minute of downloading it ends with error saying "Unable to combine settings" and it can not proceed.with Plug and Play. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 5/23/2018 1:29:18 PMNew subject after splitting |
|
5/23/2018 2:10 PM | |
Posts: 108 Rating: (4) |
Check P-set in the device and in the configuration. P-set should be the same. |
Follow us on