11/7/2020 9:50 AM | |
Posts: 2 Rating: (0) |
Attached Diagnose buffer, Please advice me: Error type: Event ID 16# 5961 Parameter assignment error in parameters for central S7 modules subrack 0 Slot 7 Error type: Slot configured for CPU is not occupied or is occupied by a place holder, or a station has failed or the switched I/O system has lost its redundancy. Data record number: 255 Operating mode: STOP (internal) External error, Incoming event 07:43:54.572 AM 11/05/2020 (Coding: 16# 5961 FF04 C17B 0064 0007 FF05) AttachmentDiagnose Blower A05112020.txt (348 Downloads) |
Follow us on