11/12/2020 10:46 AM | |
Joined: 9/25/2017 Last visit: 4/19/2024 Posts: 5 Rating: (0) |
Hi Dear RichardCarr I have a similar problem with log in/out program function in WinCC. We used on button to log in and log out, but now when we press log in it is work properly and ask for user/pass, when we press it again to log out we go log out but after that if we press log in, nothing happens. I mean log in window not appears. you can see the attachments. Any help will be appreciated. Best regards ------------------------------------------------------------------------------------------ AttachmentWord.docx (36 Downloads) |
Last edited by: omidsyt at: 11/12/2020 10:50:40Last edited by: Jen_Moderator at: 11/12/2020 12:09:30New subject after splitting |
|
11/12/2020 1:41 PM | |
Joined: 5/16/2014 Last visit: 9/12/2022 Posts: 7298 Rating: (2147)
|
Hello omidsyt, do you use WinCC V7.4 SP1 in combination with the option WinCC Audit V7.4 SP1 ? There was an issue with WinCC Audit V7.4 SP1 in combination with SIMATIC Logon. Update 16 for WinCC V7.4 SP1 and WinCC V7.4 SP1 ASIA Update 2 for Audit/ChangeControl V7.4 SP1 and WinCC/Audit V7.4 SP1
Georg Berghof |
PS: If this post did really help you, you may use the Rate-button |
|
Follow us on