10/26/2020 1:23 PM | |
Joined: 2/20/2019 Last visit: 5/2/2024 Posts: 5 Rating: (0) |
Hi, I'm trying to create a VBscript that generate some king of an alarm word with multiple external tags. Since there is no alarm word in my PLC and I cannot modify the its program, I need to create one elsewhere. I'm using a TP1500 comfort pro panel linked with a Modicon TSX premium PLC. I need to achieve something like this: Internal Tag (integer) | bit 0 = (Boolean PLC tag value X) bit 1 = (boolean PLC tag value Y) bit 2 = (boolean PLC tag value Z) and so on I am looking for a way to set specific bits address from an internal integer tag as the boolean value of an external tag. Can you guys help me? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 10/27/2020 06:41:59New subject after splitting |
|
Follow us on