11/30/2020 2:01 PM | |
Posts: 1 Rating:
|
Hi, Please help us how to define details in connection of a pc on the local
network and remote PXC100-E.D over the internet. We have checked connection with some other programs and communication with PXC100 is working fine, so connection is not an issue. Obviously, XWorksPlus needs some additional parameters to connect to PXC100. Some advice would be great. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 12/01/2020 09:56:10New subject after splitting |
|
12/1/2020 10:12 AM | |
Joined: 11/8/2017 Last visit: 7/12/2024 Posts: 328 Rating:
|
Hi, The PXC controllers do not support NAT or internal port forwarding - you may need to use a PXG3 router to handle the communications coming from / going to the internet-side of the 4G router. This was discussed previously here. For your current set up, there is no method / route available for the comms to come into the 4G router, and then be routed to the PXC controller. Regards, |
Follow us on