(0)| 12/30/2020 4:09 AM | |
|
Posts: 1 Rating:
|
connect to port X1 P2, connect via putty,user name :root password:root |
| 1/4/2021 8:24 PM | |
|
Posts: 13 Rating:
|
I understand that this is anoying: On the example image IOT2050_Example_Image_V1.0.2 The Ethernet Ports are Identified as X1-P1 and X1-P2. By default: X1-P2, the top one, has a fixed IP address 192.168.15.250 or something of the like, and does not respond to pings. X1-P1, the bottom one, is in DHCP mode. and will be assigned an address by the DNS server. In my case, I had to connect a monitor to the DisplayPort and a USB keyboard to make initials setup. A lot of issues are solved by doing.
a valid internet connection is needed. |
| 1/7/2021 9:15 AM | |
|
Joined: 4/28/2015 Last visit: 4/24/2025 Posts: 3345 Rating:
|
Hi, here you can find the instruction for the first setup of the device. Best regards! |
|
Not working for IOT2050 support anymore from March 1st, 2024. |
|
Follow us on