1/9/2021 11:07 AM | |
Joined: 9/12/2018 Last visit: 9/18/2023 Posts: 1 Rating: (0) |
Como adiciino esse hardware em uma cpu 1516/pn/dp nao estou conceguindo inserir ele ...sent from App |
1/9/2021 11:57 AM | |
Joined: 9/27/2006 Last visit: 8/7/2024 Posts: 12273 Rating: (2680)
|
Translation from the Portuguese text:
Olá Schimdt; O fórum da Siemens escolheu o inglês como idioma internacional, para reunir participantes de vários países. Escreva-nos em inglês na sua próxima visita. Hello Schimdt; The Siemens forum has chosen English as an international language, to bring together participants from many different countries. Please write to us in English on your next visit. The 6ES7-331-7TF01-0AB0 is a 4-20 mA HART analog module for the S7-300 family. It cannot be used directly in a S7-1500 configuration. However it can be used as part of a ET 200M station, connected to thr S7-1500 either over Profinet (with an IM 153-4) or over Profibus-DP (witn an IM 153-2). https://support.industry.siemens.com/cs/ww/en/view/22063748/20105841675 Hope this helps, |
Last edited by: dchartier at: 01/09/2021 11:59:01Last edited by: dchartier at: 01/09/2021 13:10:11 |
|
This contribution was helpful to2 thankful Users |
Follow us on