1/21/2021 12:31 PM | |
Joined: 4/28/2015 Last visit: 11/23/2023 Posts: 59 Rating: (0) |
Hello Experts, I have a problem with Horn activation on WinCC v7.5.1. I follow the manual and I create internal tags and I configure the horn editor as per attached file. Internal tags working correctly, when new alarm incoming variable go to TRUE and back to FALSE when alarm is acknowledge. The problem is that there is no sound.. I also add HMRT.exe on startup service. My architecture is composed by: - nr.1 eng. station - nr.2 servers - nr.4 clients Regards, Mauro Thank you, MC AttachmentHorn_problem.docx (127 Downloads) |
Follow us on