11/25/2015 11:52 AM | |
Posts: 21 Rating: (0) |
Hi, I would like to know, Is there any similarities in both software.? Thanks. |
11/25/2015 7:45 PM | |
Joined: 9/27/2006 Last visit: 8/15/2024 Posts: 12277 Rating: (2680) |
Hello jagan; What are you looking for, when you ask about similarities? Both WinCC v8 and WinCC OA are SCADA packages, both allow monitoring, control and supervision of plants and operations, both can be scaled for distributed applications (with server/client configurations and tag number upgrades), both can be connected for archiving of process data to databases and historians, both can be expanded with various optional licenses for various functionnalitiesd not in the standard package... Without details it is hard to focus on adequate replies. I suggest you open the Siemens Product webpages on Simatic SCADA software. http://w3.siemens.com/mcms/human-machine-interface/en/visualization-software/Pages/Default.aspx There are links to WinCC and WinCC OA presentations in that page, with inserted documents and videos that can probably give you pointers on the differences and similarities between the 2 packages. When you have more specific questions we may be able to help out more. Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 11/25/2015 7:48:58 PM |
|
This contribution was helpful to1 thankful Users |
6/6/2019 5:52 PM | |
Joined: 9/2/2014 Last visit: 5/17/2024 Posts: 2 Rating: (0) |
Modbus TCP/IP is supported however the version you are referring to is not currently supported. WinCC OA supported versions will cover the most recent release back to three versions. At the time I am writing this email. Here are the supported versions. V3.16 p11 (current release) V315 p19 V314 p24 If you are looking for additional WinCC OA information, I would suggest registering at the WinCC OA Portal located at https://www.winccoa.com and/or check out the KAASM WinCC OA youtube channel. Here is a link to an introduction to WinCC OA webinar https://www.youtube.com/watch?v=03w2w4y9UAA Cheers, Shawn |
Last edited by: shawsx at: 06/06/2019 17:54:45Last edited by: Jen_Moderator at: 06/07/2019 10:30:07Embedded video. Shawn |
|
This contribution was helpful to1 thankful Users |
1/24/2021 12:55 PM | |
Posts: 100 Rating: (0) |
Thanks for this description , it's really helpful |
Follow us on