1/30/2021 3:52 AM | |
Joined: 12/18/2014 Last visit: 8/7/2024 Posts: 33500 Rating: (4162)
|
Yes, it is possible that a LOGO! communicates with an S7-1200. The LOGO! be the client or the server. In my opinion, it is easier if the LOGO! the client is. LOGO! - S7 Connection with LOGO! Client and S7-1200/1500 Server |
This contribution was helpful to2 thankful Users |
1/30/2021 6:11 PM | |
Joined: 12/27/2018 Last visit: 3/7/2024 Posts: 99 Rating: (2) |
Thanks very much! |
Follow us on