1/16/2021 5:26 PM | |
Joined: 11/17/2010 Last visit: 9/11/2024 Posts: 105 Rating:
|
Hello! Please, Can anybody help me with the scenario below? Scenario - IOT2040 with example image from Siemens.
When I reboot the IOT, the system can get both the static IP address and the dynamic one BUT now I show the problems: - Sometimes after a few hours, the IOT lost the static IP address, keep the dynamic but "disable SSH access" and don't response do PING requests, for both X1 and X2 physical interfaces. Informations Some people recommends anothers to create a virtual interfaces but the Yocto Poky seems to not permit this workaround. EDIT - ADDED INFORMATION This IOT is running and something strange happened: without any command or change, he lost their static IP for X2 interface and got a new one from DHCP server present on the network. I'm adding the log files to someone could help. Attachmentmessages.txt (287 Downloads) |
Last edited by: esantos at: 01/17/2021 00:08:55Best regards, |
|
1/18/2021 2:42 AM | |
Joined: 11/17/2010 Last visit: 9/11/2024 Posts: 105 Rating:
|
Please! Could someone help me? Thanks!!! |
Best regards, |
|
2/4/2021 6:32 PM | |
Joined: 12/12/2016 Last visit: 4/8/2024 Posts: 640 Rating:
|
Hello Eduardo, Sorry for the late reply. I am unable to reproduce this with the local DHCP Server I setup but its indeed a strange behavior if eth0:0 is losing the config regardless if its the DHCP or static setting on your side. I would suggest to please open an issue on here for the image-devs to take a closer look. Best regards! |
Follow us on