2/5/2021 3:13 PM | |
Joined: 3/14/2008 Last visit: 4/26/2024 Posts: 2066 Rating: (927)
|
Hi, I don't think you can do something about it. I think it makes sense because in BATCH recipe, you can start a phase multiple times with the same control strategy. The prepared list will be taken over during the next validation of the control strategy and it's setpoints (PARAM check). It is not the actual CS that is shown there. Also, its an OCX control which cannot be edited. There are a few properties like color, metric sizes that can be adjusted, but not much more.
|
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to2 thankful Users |
Follow us on