2/9/2021 10:06 PM | |
Joined: 6/1/2018 Last visit: 10/28/2022 Posts: 4 Rating: (0) |
Hoping someone has overcome this issue. We need to extract alarm archives from an OS server pair using an OpenPCS7 machine. Both machines are on the same subnet and a single domain user with admin privileges is used on both machines. Using the WinCC OLE DB Provider on a Powershell script with the Fill command receives the error: Exception calling "Fill" with "1" argument(s): "'WinCCOLEDBProvider.1' failed with no error message available, result code: E_FAIL(0x80004005)." The connection string is Provider=WinCCOLEDBProvider.1;Catalog=CC_OS1_21_01_07_14_03_51R;Data Source=OS_Prj_OS1::\\WinCC Query is: "ALARMVIEWEX: SELECT * FROM AlgViewExEnu WHERE DateTime > '2021-02-09 06:00:00' AND DateTime < '2021-02-09 06:00:00' ORDER BY DateTime ASC" I've attached the PS script Pcs7 V9.0 SP2 Win 2016 AttachmentPCS7AlarmExport_Upload.txt (210 Downloads) |
Follow us on