2/16/2021 11:15 AM | |
Joined: 12/20/2019 Last visit: 7/24/2024 Posts: 59 Rating:
|
the respective result texual interconnection tab. |
2/16/2021 11:26 AM | |
Joined: 12/20/2019 Last visit: 7/24/2024 Posts: 59 Rating:
|
The MLFB is: 6ES7 321-7BH01-0AB0 |
2/17/2021 5:38 PM | |
Joined: 9/1/2017 Last visit: 7/9/2024 Posts: 156 Rating:
|
Hi The conclusion of our discussion must be that your hardware does not match with your pcs7 version,but: I checked siemens compatibility tool which says 6es7-321-7bh01-0ab0 is compatible with step7 v5.5 sp1 and 6es7-321-7bh01-0ab0 v2 is compatible with step7 5.4 sp3 So there is no matter with all pcs7 v8 variants. It also exist in PCS7 Released Modules (V8.0 SP2). At last i tried some test with pcs7 v8.0 upd1 and v8.0 sp2,using s7-400/400H and ET200M. Depends on which IM i used, 6es7-321-7bh01-0ab0 can be find im pcs7 or standard profile of hw config. I tested both case and there were no problem in compilation and generating module drivers. So, If it is possible you can send your project. If not test your project in another pcs7 system. And finally you can handle your channel driver manually Hope this helps Regards Hosein |
This contribution was helpful to
1 thankful Users |
Follow us on