2/17/2021 8:08 PM | |
Joined: 1/20/2012 Last visit: 3/19/2024 Posts: 15 Rating: (0) |
Hi, that option was already on, otherwise it wont start. So yes, the sf failure led is still blinking. Regards |
2/18/2021 2:28 PM | |
Joined: 11/15/2017 Last visit: 3/21/2024 Posts: 78 Rating: (15) |
What Firmware version does the PLC have? |
2/18/2021 3:10 PM | |
Joined: 1/20/2012 Last visit: 3/19/2024 Posts: 15 Rating: (0) |
See attachment, it is a printscreen when I download something.
|
2/18/2021 4:35 PM | |
Joined: 11/15/2017 Last visit: 3/21/2024 Posts: 78 Rating: (15) |
FW version 2.8 is not suppported by TIA 15.1, you need to use TIA V16 for that. But you could also try downgrading the firmware, which is pretty easy using TIA Portal. Download the Firmware file (https://support.industry.siemens.com/cs/document/109478459/) Edit: I'm not sure this fixes your problem, but it's worth a shot. |
Last edited by: Sibrand at: 02/18/2021 16:36:53Last edited by: Jen_Moderator at: 02/19/2021 08:28:53Embedded video. |
|
2/22/2021 11:50 AM | |||
Joined: 3/11/2019 Last visit: 4/26/2024 Posts: 1378 Rating: (244) |
Hi FastFietser2, please check the diagnostics buffer of the cpu/post the diagnostics buffer here (not the module diagostics). Online & Diagnostics -> Diagnostics -> Diagnostics buffer -> Save as. I assume there is another/additional difference in the configuration, as the CPU 6ES7 515-2FM02-0AB0 is compatible to 6ES7 515-2FM01-0AB0. The "Additional Info" in the module diagnostics, is always shown. Also the message in download dialogue to the difference is always shown, but can be ingored. CPU 1515F-2 PN, 750KB Prog.,3MB Data
regards sancruz |
||
Last edited by: sancruz at: 02/22/2021 11:53:58Last edited by: sancruz at: 02/22/2021 11:54:57Last edited by: sancruz at: 02/22/2021 13:10:50Feedback appreciated, please rate |
|||
Follow us on