3/9/2021 8:31 AM | |
Joined: 4/6/2018 Last visit: 5/12/2024 Posts: 33 Rating: (0) |
Good day. We receive data via the Modbus TCP protocol on the TP1200 Comfort panel from the Scadapack32 PLC. There is a problem getting this String type. The line that should look like "03 03 2018" looks like "32 0 2 2 10" for us. At the same time, on another C-More panel, the line is displayed correctly "23 03 2018". I can assume that Siemens, as usual, counts the bytes from the back side. Is it possible to configure the correct display of the string without using a script? AttachmentASCII.zip (99 Downloads) |
Follow us on