3/10/2021 10:51 AM | |
Joined: 6/14/2013 Last visit: 3/18/2023 Posts: 218 Rating: (9) |
Hi all, I have fault in cpu 315. Here diagnos. Please help. Thanks. AttachmentDiagnose.txt (282 Downloads) |
3/10/2021 2:36 PM | |
Joined: 9/27/2006 Last visit: 4/27/2024 Posts: 12257 Rating: (2665)
|
Hello mirip; One important point: most members of the forum come from countries that do not speak French, that could be a problem to understand the contents your diagnostic file. You should be able to change the language of your Step 7 project from French to English, for example: https://support.industry.siemens.com/cs/ee/en/view/8795118 Next: you mention in your post that you have a CPU 315, your diagnostic buffer header states that the file was taken from a CPU 318-2 (6ES7 318-2AJ00-0AB0). Could you clarify this, a CPU 318 is a S7-400 in disguise, and some error codes do not apply to a CPU 315. Starting at entry #20, you have a recurring message that is coded in Hexadecimal, "No entry in the text database", with an error codes 16# E0CC, 16# E000 or 16# E21F which I cannot recognize and are not part of the standard error codes for S7-300 CPUs, as far as I know You can download the description of error codes for Step 7 in the following link: https://support.industry.siemens.com/cs/ee/en/view/770453 Given these special error codes, it could be a good idea to contact Siemens techs directly about this situation, using a Support Request (link at the top of this page). If you have an English version of the duagnostic buffer it would be useful, for them as well. Give them a description of the status of the CPU and any strange behavior it exhibits. Hope this helps, |
Last edited by: dchartier at: 03/10/2021 20:29:58 |
|
This contribution was helpful to1 thankful Users |
3/10/2021 4:31 PM | |
Joined: 6/14/2013 Last visit: 3/18/2023 Posts: 218 Rating: (9) |
hi dchartier, thanks. You are right, it's a speed7 vipa 315 SB, not siemens, but even caracteristics. mirip. |
3/10/2021 6:17 PM | |
Joined: 6/14/2013 Last visit: 3/18/2023 Posts: 218 Rating: (9) |
Thank you dchartier, I'll see with VIPA. mirip. |
Last edited by: mirip at: 03/10/2021 18:19:15 |
|
3/11/2021 7:16 AM | |
Joined: 6/14/2013 Last visit: 3/18/2023 Posts: 218 Rating: (9) |
Hi, What is replacement for VIPA CPU 315-SB Hardware in SIEMENS portfolio? mirip |
3/11/2021 12:03 PM | |
Joined: 9/27/2006 Last visit: 4/27/2024 Posts: 12257 Rating: (2665)
|
Hello mirip; Marcjan is correct, but the S7-318 line of CPUs has been completely discontinued since 2018, no spare parts, no repairs (by Siemens directly). This article proposes different S7-300 and one S7-1500 CPUs that can be selected to replace a CPU 318-2DP. But these are not direct replacement modules, they must be configured and commissioned anew, and the program will have to be re-examined, especially if it has been designed for a Vipa CPU.. https://support.industry.siemens.com/cs/ww/en/view/109756615 Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 03/11/2021 12:09:17 |
|
This contribution was helpful to2 thankful Users |
Follow us on