3/12/2021 3:48 PM | |
Joined: 8/1/2019 Last visit: 7/9/2024 Posts: 300 Rating:
|
How to end and delete this control recipe? Its not aborting!!! It should ignore the sfc status and just abort... |
3/12/2021 4:52 PM | |
Joined: 3/14/2008 Last visit: 7/12/2024 Posts: 2076 Rating:
|
Hi, A batch can be aborted if the unit and underlying equipment is in the correct state. If you take a sfc on hand , the batch cannot be aborted. Best remedy is to solve it at the phase , make sure the phase can be aborted, then you can abort the batch. If nothing works you can open the parameter screen of the Unit_PLC block and reset/abort the phases from there, maybe then it will succeed. |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to
2 thankful Users |
Follow us on