11/16/2020 1:23 PM | |
Joined: 12/10/2018 Last visit: 6/27/2024 Posts: 109 Rating: (11) |
Hi dear friend Of course it is possible. According to the attachments, you can use two sitops (220VAC to 24VDC) Power supplies as redundant configuration. AttachmentSitop.pdf (467 Downloads) |
1/11/2021 5:26 AM | |
Joined: 5/28/2008 Last visit: 9/9/2024 Posts: 4515 Rating: (839) |
Hello, Although happening of this case is reer. I mean here deffective redundnacy module, but there is a solution to use two redundnacy module instead of one. Simply:
Please follow section 9.1; see fig. 9.2 & 9.4 of the following manual: Hope this helps. |
Ayman Elotaify |
|
Follow us on