10/12/2016 2:19 PM | |
Joined: 6/2/2009 Last visit: 2/13/2025 Posts: 61 Rating:
|
Dear all, Context: We use Profinet communication. TheS7-1500retrieves20 DWordsfrom all the30 S7-1200on the field to updateWinCC. TheS7-1500also sends2 DWordsto all the30 S7-1200on the field fromWinCC. All 30 S7-1200 have their own electrical panel and do their own process. Note: We use DWords to save communication bandwidth between S7-1500 and S7-1200. Also we use DWords to save Powertags between S7-1500 and Rack-PC supervisor WinCC DWords contain statuses, faults, memories... (not only DI / DO) Question: As we need to send a lot of information bits between S7-1200 PLCs and the S7-1500, I suppose that IODevice exchange is not a good choice.Better to send / receive DWords ? So do we need to avoid to configure our 30 S7-1200 PLCs as IODevice ? Or to configure them (S7-1200) as IODevice doesn't affect SEND_C / RECEIVE_C communication ? What is more preferable ? Is there a native way more suitable to exchange those DWords (contained inside external DBs of each S7-1200) ? Thanks in advance, David AttachmentL3P4A-WRK-DRW.docx (97 Downloads) |
10/19/2016 11:58 AM | |
Joined: 2/27/2014 Last visit: 3/27/2025 Posts: 689 Rating:
|
Hello, For Virtual IO memory it always IW and QW in TIA portal. See the attached video for better understanding. If you feel this post is useful then don't forget to rate it. AttachmentIDEVICE.zip (83 Downloads) |
With Best Regards, |
|
Follow us on