8/16/2014 10:20 AM | |
Joined: 11/21/2007 Last visit: 3/14/2024 Posts: 2323 Rating: (306) |
Hello Dempsey08 Sorry I do not have a 6RA24 available for physical checking, but I could not find any mention of the Color of the "PROG" LED in the 6RA24 Manual with me. Pl See extract of the manual attached. Can you please post the part of the manual that mentions the color of the PROG LED ? Thanks Cheers Navnag Attachment6RA24_Optional_Operator_Panel.pdf (522 Downloads) |
There is no such thing as the last bug in a program |
|
8/16/2014 4:19 PM | |
Posts: 767 Rating: (69) |
Hello Navnag, I sent you an attachment. |
8/16/2014 6:12 PM | |
Joined: 11/21/2007 Last visit: 3/14/2024 Posts: 2323 Rating: (306) |
Hello Dempsey08 Does this ever glow "Green" ? if not then maybe the LED is "RED" only You can just verify if the LED is glowing as per the conditions defined in the manual. Cheers Navnag |
There is no such thing as the last bug in a program |
|
8/16/2014 7:36 PM | |
Posts: 767 Rating: (69) |
Hello Navnag, Ok I will check your advice and if I find the solution I'll write in this forum. |
This contribution was helpful to1 thankful Users |
Follow us on