12/2/2016 8:22 PM | |
Posts: 1 Rating: (0) |
hello I have problem like Vladich problem. My HSC is enable and the input filter is minimum but the 1200 CPU loss encoder pulse when the frequency is about 500Hz but when frequency is so low and I rotate the encoder very slow by my hand the PLC can count the pulse Encoder have x , y and z output pulse I choose A/B counter the encoder generate 1000 pulse per each rotation CPU is 1200 1214AC/DC/RLY please help me excuse me for poor language ------------------------------------------------------------------------------------------ |
Last edited by: ahmad_hf at: 12/2/2016 8:23:01 PMLast edited by: Min_Moderator at: 12/3/2016 12:19:54 PMNew subject after splitting |
|
12/23/2016 7:49 PM | |
Posts: 113 Rating: (22) |
Input filter, check the settings. |
This contribution was helpful to1 thankful Users |