Industry Online Support
Technical Forum
8/21/2017 12:31 AM | |
Joined: 9/29/2016 Last visit: 1/28/2024 Posts: 1 Rating: (0) |
Siemens 1200 - telegram 111 - v90pn Hello, They lose for my English .... I have a problem ... i need leave ... siemens 1200 with v90pn drive communicating in profinet with telegram 111. I can not control the drive, as if they did not communicate ... It seems that the sina_pos block does not communicate with the drive; For example if I generate an alarm by activating the emergency in the assistant I see the bit 3 of the zsw1 that takes to 1 but i do not see it in the sina_pos_db (do not take the picture I have taken unplugged ...) The profinet link is there The telegram is set Id is set correctly Why the 1200 does not communicate with the v90 ?? What am I sleeping ??? Firmware cpu 1200 4.2 Tested firmware 1.003 and 1.01 Thanks in advance Attachmentpictures.zip (419 Downloads) |
Last edited by: Jen_Moderator at: 8/22/2017 11:05:42 AMAdded all images as an attachment. |
|
This contribution was helpful to1 thankful Users |
Follow us on