2/6/2025 10:57 AM | |
Joined: 8/3/2009 Last visit: 2/7/2025 Posts: 14670 Rating:
|
Hello AutoGen_12877 Do I understand correctly you want to show or use the amount of unacknowledged Alarms outside the Alarmcontrol? Or do you want to use the clicking event of the Button for something else? (for this there is a systemfunction and its quite easy ) If you want to use the Number of unack alarms then you can use an alarmsubscription like in the toolbox for the alarm indicator: https://support.industry.siemens.com/cs/de/en/view/109770480 Bye Murof |
If this Information really helps, you could use the Rate function |
|
2/6/2025 1:56 PM | |
Joined: 11/28/2024 Last visit: 2/7/2025 Posts: 23 Rating:
|
Hi Murof, I want to show the number of unacknowled alarms outside the Alarmcontrol on a different screen. On a different screen I have a symbolic i/o field and when the [13] Button - Single acknowledgement is clicked on the alarm control screen the number decrement should reflect on the other screen as well. |
Follow us on