3/10/2018 6:25 AM | |
Joined: 12/23/2011 Last visit: 11/22/2022 Posts: 143 Rating: (0) |
I have questions about network architecture and configuration in Netpro. Is the configuration correct? in the page61 and 63 manual SIMATIC Process Control System PCS 7 Fault-tolerant Process Control Systems siemens there are 2 Solutions for the plant bus My system is redundant, fault-tolerant plant bus or not? Why in our system for each server, there are two 1623 cards installed, but next to each CPU is one card 443-1 Is this correct? Attachmentfiles.zip (250 Downloads) |
Last edited by: PLC2011 at: 3/10/2018 6:47:22 AMLast edited by: PLC2011 at: 3/10/2018 6:50:22 AMLast edited by: Jen_Moderator at: 3/12/2018 1:23:30 PMDeleted links and added all files as an attachment. Optimized link. |
|
Follow us on