1/29/2015 9:53 AM | |
Joined: 10/11/2006 Last visit: 5/27/2024 Posts: 5853 Rating: (793)
|
Hello, the 1PH6 could be replaced with the current motor range 1PH8 which is available in synchronous and asynchronous technology. For a best possible motor dimensioning the tool SIZER is to recommend. Thus the current motor 1PH6 could be checked and the calculation of the degree of capacity utilisation is possible. A 1PH8 motor can be select and also the system components like controller, cables etc.Please ask your SIEMENS partner: http://www.automation.siemens.com/aspa_app/ |
With best regards, |
|
1/29/2015 2:22 PM | |
Joined: 10/11/2006 Last visit: 5/27/2024 Posts: 5853 Rating: (793)
|
Hello, there is no direct substitution type available. So you have to compare the characteristics of 1PH6 with 1PH8 and than you can choose a suitable 1PH8. Options 1PH6: Option K83 means: Terminal box rotated through 90°; cable entry from A (by 1PH8 on request) Option L41 means: Paint RAL 9005 Option M11: I don´t know Used encoder: ROD_431 (HTL-encoder with 1024 impuls./rotations) A possible MLFB could be: 1PH8103-1HF03-1BA1-Z X-Colours Note: This 1PH8 has PN=5,5kW, nN=1500rpm, 35NM. Please check thedata whether a replacement is possible. AttachmentD:\Motoren\1PH6101-4.G5.pdf (447 Downloads) |
With best regards, |
|