6/22/2010 9:01 AM | |
Joined: 6/3/2009 Last visit: 1/13/2025 Posts: 101 Rating:
|
Dear Forum Member I have S7-400 H system with 2 CP443-1, 1 CP441-2 is communicatingvia profibus to5 IM-153. The above system is connected(VIA ISO) to2 PC(WINCC) are working fine. I had made redundancy connection toPLC to PC working fine. but i requries CP443-1 redundancy connection? How to do it.......... Help Me........... I had Attached my hardware configuration and overview. AttachmentDetail.zip (222 Downloads) |
6/22/2010 11:13 AM | |
Joined: 6/3/2009 Last visit: 1/13/2025 Posts: 101 Rating:
|
Dear Tagolover Two cp443-1 in each cpu rack to be redudant individually is my requriment. I hope this may be clear. |
6/22/2010 11:40 AM | |
Joined: 9/7/2007 Last visit: 10/9/2024 Posts: 550 Rating:
|
Have a look for thisnetwork topologyit may help you in configuration AttachmentSCALANCE.pdf (264 Downloads) |
Last edited by: Khaled_Ezzat at: 6/22/2010 11:51 AMLast edited by: Khaled_Ezzat at: 6/22/2010 11:50 AMBest Regards |
|
Follow us on