10/1/2007 8:40 AM | |
Posts: 1776 Rating: (95)
|
Hi, ateam have described all possibilities April |
10/1/2007 2:55 PM | |
Posts: 1275 Rating: (123)
|
Hi Navid... Weird thing happened at the forum: I read an answer from you, and when I tried to reply there was a system problem.... and now your answer is gone, I refresh the screen and it's as if it had never been posted.. either there was a problem or I'm going crazy! The answer I somehow read was saying that it would be good if there was a way to use a set of mouse, video and keyboard which could be used to control 2 PC's... and there is.. check this KVM switches site. And the definition of KVM in wikipedia. But the downside to this is the user would have to switch systems to check for alarms... Like I said, if you have only 1 project, you could get all alarms, or at least the critical ones, for both systems. This way, if a user is operating area 1, area 2 will still be monitored for critical faults. Best regards, Danielle |
4/1/2014 1:01 PM | |
Joined: 9/1/2005 Last visit: 12/5/2024 Posts: 4114 Rating: (195) |
follow up question published by pk2_kdhis split to a seperate thread with the subjectMointoring of 2 PLC's with different IP series in 1 PC. Best regards CS Moderator |
My Forum is the place to personalize your profile, |
|
Follow us on