Industry Online Support
Technical Forum
1/28/2012 1:09 PM | |
Joined: 11/21/2007 Last visit: 5/31/2023 Posts: 2321 Rating:
|
Hello You have not mentioned which CPU ypu are using. Most Commonly used CPUs with 2 PG PortsisCPU 928B. Well there are some restrictions on operating two PG Ports in parallel. I have attached an extract from Manual of CPU 928B which gives details of the same. Pl refer to Table 11.3 for a summy of the restrictions. Hope this helps Cheers Navnag AttachmentParallel_Operation_of_2_PG_Interfaces.pdf (89 Downloads) |
There is no such thing as the last bug in a program |
|
1/31/2012 9:12 AM | |
Posts: 9 Rating:
|
Thankyou ! Will. |
Follow us on