8/28/2019 11:17 AM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating:
|
hi again, I found something in an other forum. Seams that I was rigth and this is a costumized CPU. As per other pages this should be a DC/DC/DC PLC with just more RAM. You can try to project it as 6ES7215-1AG40. hope this helps, regards, |
FCK WAR! |
|
This contribution was helpful to
2 thankful Users |
8/7/2021 9:47 PM | |
Posts: 1 Rating:
|
I have same PLC and is not possible upload anything, event i need force and test few IOs and nothing, Even using ES7215-1AG40. with Tia 14 or Tia 16. May be trying with TIA 17 ??? |
8/8/2021 12:45 AM | |
Joined: 3/16/2015 Last visit: 10/10/2021 Posts: 1250 Rating:
|
It will not work. You either get the HSP from Siemens or the manufacturer or fix the machine without plugging in. Nothing else will work. |
Follow us on