10/9/2020 1:02 PM | |
Posts: 2 Rating: (0) |
Good day I have the following fault on the Atlas Copco GA11vsd FF, Compr, Motor Convert.Timeout, i in inadvertently wiped the parameters, has some one got a list that will share so i an get the unit to start again. I am sure it is the parameters in the Micromaster 440 Norman ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 10/12/2020 07:35:03New subject after splitting |
|
10/26/2020 8:19 AM | |
Posts: 2 Rating: (0) |
Hi GA11 VSD FF SET 9824-0729-9102 Thx |
1/13/2022 7:21 AM | |
Joined: 3/25/2008 Last visit: 10/4/2024 Posts: 194 Rating: (8) |
Hi here you have the file you just need to change the .txt extension to .dnl so I can succeed with the recovery of the compressor
Attachment9824-0729-91 02.txt (1138 Downloads) |
This contribution was helpful to1 thankful Users |
7/21/2022 2:38 PM | |
Joined: 3/25/2008 Last visit: 10/4/2024 Posts: 194 Rating: (8) |
hello, what parameter set is there? |
10/26/2022 2:40 PM | |
Joined: 11/26/2020 Last visit: 10/31/2023 Posts: 7 Rating: (0) |
Hello. Where can I see this number ? |
Follow us on