11/19/2020 4:23 PM | |
Joined: 10/11/2006 Last visit: 6/5/2024 Posts: 5857 Rating: (793)
|
Hello, It is possible to use isochrounous mode and Tel. 105 + Tel. 750. It is described in the manual: 4.1.2.2 Configuration - Data exchange with the drive (S7-1500, S7-1500T) https://support.industry.siemens.com/cs/ww/en/view/109766462 Supplementary data Select the "Torque data" check box if you want to configure the data connection of the torque data. If you have selected a drive with which the additional telegram 750 has been configured, the "Torque data" check box is preselected. 3.7.1 PROFIdrive-Telegrams (S7-1500, S7-1500T) |
With best regards, |
|
Follow us on