3/2/2016 10:37 AM | |
Posts: 22 Rating: (0) |
Hi all, I have a CPU 1241 AC/DC/Relay and external 24VDC power. Can I connect the negative pin of 24VDC to 1L and 2L of PLC output terminal. In system manual, the diagram only shows connection of +24 to 1L and 2L ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 3/2/2016 2:26:17 PMNew subject after splitting Last edited by: lezard at: 3/2/2016 2:46:19 PM |
|
3/2/2016 8:54 PM | |
Joined: 3/16/2015 Last visit: 10/10/2021 Posts: 1250 Rating: (173) |
Yes you can. L1 and L2 are common terminals of the relays. |
This contribution was helpful to2 thankful Users |
Follow us on