2/14/2022 1:01 PM | |
Joined: 1/15/2022 Last visit: 10/16/2023 Posts: 13 Rating: (0) |
Hello, I have two S7-1200 PLC connected with Modbus RTU. I will use the slave as remote I/O. I have read the Article "How do you establish a MODBUS-RTU communication with STEP 7 (TIA Portal) for the SIMATIC S7-1200?" How do you establish a MODBUS-RTU communication with STEP 7 (TIA Portal) for the S... - ID: 47756141 - Industry Support Siemens How do I obatin/use the data from the slave, in the master PLC? I would like to activate relay outputs in the master PLC from inputs in the slave PLC. (Inputs in slave will activate outputs in master PLC). Regard Martin |
Last edited by: Jen_Moderator at: 02/15/2022 08:36:37Optimized link. |
|
Follow us on