8/4/2022 10:26 PM | |
Joined: 1/17/2022 Last visit: 9/4/2023 Posts: 27 Rating: (0) |
good greeting I hope you are in good health I had a problem with PLC 412-2DP The program was lost from the PLC and the program was printed again and the program was downloaded to use all units, as shown in the attached picture Note that I have verified all addresses for units Please help if possible. Thank you very much ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 08/05/2022 07:10:13New subject after splitting |
|
8/9/2022 4:47 PM | |
Joined: 1/17/2022 Last visit: 9/4/2023 Posts: 27 Rating: (0) |
This is a group of blocks uploaded to PLC as in the picture The attached file is the structure of the program Do you have any comments? Thanks a lot for the help
AttachmentProgram_Structure.pdf (686 Downloads) |
Follow us on