8/31/2022 1:48 PM | |
Joined: 8/31/2022 Last visit: 9/1/2022 Posts: 1 Rating: (0) |
Hi there, We are having the same problem here, but the drive didn't reach 20% to trip, just when we start the drive, it's directly shows "A1 DC Bus Over Voltage", and we've done things from our side are swap and replace power cell, replace output CT, replace output attenuator resistor and even we replace all card in the control section. The motor also disconnected from the load, which still didn't solve this problem. If you've solved this problem, kindly tell me how to solve this, thank you before. ------------------------------------------------------------------------------------------ |
Last edited by: ibnusani at: 08/31/2022 13:52:40Last edited by: ibnusani at: 08/31/2022 13:55:51Last edited by: Jen_Moderator at: 09/14/2022 10:18:07New subject after splitting. Quote inserted. |
|
Follow us on