10/17/2022 11:58 AM | |
Joined: 12/22/2012 Last visit: 6/4/2024 Posts: 91 Rating:
|
I decided to follow sample project. But I need to use an external encoder to measure the web length. Original sample system uses IM155-6PN as remote IO modules instead of ordinary modules at the right side of CPU. Does it have a meaning, benefit? What is the reason to manage a remote IO configuration rather than to insert IO modules to the right side of CPU?. [snip] Note: the sample project is 109744840_FlyingSawBasic. I really appreciate for quick advices. . . ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 10/18/2022 08:04:11New subject after splitting. Division of questions into separate topics. Last edited by: Jen_Moderator at: 10/18/2022 08:05:19Embedded image added. |
|
10/18/2022 11:37 AM | |
Joined: 12/22/2012 Last visit: 6/4/2024 Posts: 91 Rating:
|
Dear Jen, I can use one of the 5V or 24V encoder to use as incremental or pulse generator. I did not buy any encoder yet. I just wanted to know what is the difference of module. it is necessary only for web length measurement. But I have several questions about sample project 109477745. I feel grateful a lot if you help me. 1) I wanted to change the cpu 1511T instead of 1515T due to limited budget reason. But I got the following warning. What is the reason of that "Profinet Interface not supported"? Can I replace it? Because I have only one V90 servo drive which needs heavy communication load. 2) Why the system configured with distributed IO modules? It is also possible to insert necessary module to right side of main CPU. Is there any reason? I really appreciate i I get answers asap because of I have to order all items asap. thanks in advance |
Follow us on