11/13/2022 6:37 PM | |
Joined: 8/31/2022 Last visit: 5/29/2024 Posts: 11 Rating: (1) |
Hi everyone, I'm having a problem with system alarms. In the attached screenshot it is visible that the text shows special characters probably used to make the text itself dynamic. Unfortunately in the documentation I could not find useful information on how to solve it, I tried to change the display language but it not solved the problem. My setup is: TIA Portal V17 update 5 on Windows Server 2016 Standard Build 14393. System Language: IT Runtime Language: IT and EN Any suggestions? BR, LF
AttachmentAlarmScreenshots.zip (396 Downloads) |
Last edited by: luciano.fab at: 11/13/2022 18:40:37 |
|
11/14/2022 10:35 AM | |
Joined: 8/31/2022 Last visit: 5/29/2024 Posts: 11 Rating: (1) |
I'm sorry but in the attached document the Windows Server 2016 Standard operating system is considered compatible. Where is the mistake? AttachmentMicrosoft-Windows-Server_en_2022-10-25.xlsx (315 Downloads) |
Last edited by: luciano.fab at: 11/14/2022 10:39:54 |
|
11/14/2022 11:20 AM | |
Joined: 2/3/2022 Last visit: 4/23/2024 Posts: 304 Rating: (27) |
Hi! You are right! I did not check the correct information. I will see if I can find something that will help you. Br! |
Follow us on