11/24/2022 5:05 PM | |
Posts: 4 Rating: (0) |
Hi, Currently I am involved in an “Obsolescence Project”, meaning upgrading control system hardware that is obsolete and spares are no longer available. The vendor for a particular scope of the project dealing with Siemens based control panels is recommending that almost all the component be replaced, due to their lifecycle either being obsolete or active/mature. Part No below This is a two part question: [snip] Part 2. Items (8) thru (11) are ET-200M components which are scheduled to be phased out in Oct 2023, meaning spares will be available fora minimumof 10 years. Given the size of the install base it is likely Siemens will continue to have spares available for a much longer time. The replacement unit, ET-200MP, while appearing similar is quite different, the Remote Module, all IO, even the mount DIN rail have to be replaced. What is your opinion for migrating to ET-200M today? Couple of key notes.
Many Thanks for suggestions. ( 1 )-Siemens:6AV7875-0AC20-1AC0 Description:HMI, PC677B ( 2 )-Siemens:6AG1412-3HJ14-4AB0 Description:CPU S7-412 ( 3 )-Siemens:6AG1341-1CH02-7AE0 Description:CP (comm module, RS422/485) ( 4 )-Siemens:6AG1443-1EX11-4XE0 Description:CP Comm ( 5 )-Siemens:6AG1407-0KR02-4AA0 Description:Power Supply ( 6 )-Siemens:6AG1400-2JA00-4AA0 Description:CPU Module Rack ( 7 )-Siemens:6EP1337-3BA00 Description:PS SITOP PSU100M ( 8 )-Siemens:6AG1153-2BA02-7XB0 Description:Rem IO ET 200 ( 9 )-Siemens:6AG1321-7TH00-4AB0 Description:IO - Digital Input ( 10 )-Siemens:6AG1322-8BF00-2AB0 Description:IO - Digital Output ( 11 )-Siemens:6AG1331-7KF02-2AB0 Description:IO - Analogue Input ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 11/25/2022 07:55:23New subject after splitting. Division of questions into separate topics. |
|
11/25/2022 12:07 PM | |
Joined: 8/12/2021 Last visit: 10/3/2024 Posts: 324 Rating: (30) |
Hi KTexh! Maybe our technical support colleagues can help you with this issue. Here you can find the official product information for migration.
|
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to1 thankful Users |
Follow us on