7/7/2023 10:29 AM | |
Joined: 2/17/2020 Last visit: 7/11/2024 Posts: 1019 Rating:
|
Hi JPALC, For the PLC programming, you need the license STEP 7 Professional V18 (TIA Portal). For the HMI application (Runtime) programming, it really depends on whether you want to configure an Advanced, Unified PC or Professional Runtime. I recommend you review the order list in the following link, since it also depends on the number of PowerTags (tags that the RT will exchange with the controllers) configured: Delivery release SIMATIC WinCC V18 If the RT is to be run on a different PC than the engineering PC, you will also need a separate Runtime license (Advanced, Unified PC or Professional). |
A rating will be well appreciated. |
|
7/7/2023 10:50 AM | |
Joined: 3/30/2020 Last visit: 7/11/2024 Posts: 4623 Rating:
|
Perhaps try the [TIA Selection Tool]. Select the products that you want to use. Then have the cloud service recommend which software and licenses with fit the devices. |
Activities of this user is voluntary. There is no obligation or liability placed on this user. Though optional, your 'please' and 'thank you' is highly valued. |
|
7/7/2023 12:55 PM | |
Joined: 2/23/2023 Last visit: 1/16/2024 Posts: 2 Rating:
|
The project is to controlate several ligh.turning on and off since touch screen. I think that for this, WinCC advanced is better because it is like a HMI |
Follow us on