3/11/2024 3:43 PM | |
Joined: 5/6/2022 Last visit: 10/14/2024 Posts: 465 Rating: (92) |
Hi mdarende, Unfortunately this functionality is not available in the standard user management of the TIA Portal (force password change that I know of), I only see it possible that using the online permissions management they could log in the first time and update their password: "SIMATIC HMI WinCC Unified Engineering V18: Editing password, status or role" However, with UMC there are two ways: First one, if you create a user from the UMC web interface, there is a column titled "Must change password" where you have to check it to True. In case the user is created in the AD, you can set this condition up in the AD server. Best regards! |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to1 thankful Users |
Follow us on