6/6/2018 9:41 AM | |
Joined: 4/28/2015 Last visit: 6/5/2023 Posts: 9534 Rating:
|
Hello, in case your CPU with CP is Slave you don't need configure Master on cfg. What I remember from my old prjs, only defined I/O table with correct data types and length, then correctly use DP_READ/WRITE instructions in my code with I/O buffer. Nothing special. Update: I expect same comm settings (speed, unique address, profile) for Profibus set to CP module. Update2: some Example which can be helpful to you: Configure S7-300 with CP 342-5 DP Master/Slave |
Last edited by: Duris_I at: 6/6/2018 9:43:34 AMLast edited by: Duris_I at: 6/6/2018 9:44:03 AMLast edited by: Duris_I at: 6/6/2018 9:56:44 AMWith best regards... |
|
6/6/2018 3:42 PM | |
Joined: 6/27/2016 Last visit: 5/26/2023 Posts: 33 Rating:
|
Darius, Thanks for your help, the fault was the profibus cable |
Follow us on