3/18/2024 2:11 PM | |
Joined: 6/16/2023 Last visit: 3/4/2025 Posts: 9 Rating:
|
Hi, I am comisioning a S7-1200 and TP1200 comfort panel, i have downloaded to both devices and I can access them through tia portal and by pinging them. The problem is that the HMI does not want to communicate with the PLC and gives me error 190011 when I try to send bits. I can't think why that is the case and I could not find anything online, and I made sure that the tag connection is correctly defined for my tags. I have a connection between the devices through TIA portal set with the ETHERNET interface. And no password set for the PLC. One thing that I am not sure of is the access point setting, currently it is set to ''S7ONLINE'' but I am not sure If i need to change this. Both devices are completely new out of the box, i have also updated the image on the panel to V17.x The transfer setting in the panel settings is also set to PN/EI. And the IO device in profinet setting is OFF. is there anything else i would have to do to configure this communication? |
3/18/2024 2:24 PM | |
Joined: 3/28/2023 Last visit: 2/26/2025 Posts: 27 Rating:
|
What HMI version are you using? It's been mentioned in other posts, try updating the time on the PLC and HMI so they're the same. https://support.industry.siemens.com/forum/ca/en/posts/wincc-v17-update6-runtime-don-t-work/299144/?page=0&pageSize=10#!#post1145901 |
This contribution was helpful to
1 thankful Users |
3/18/2024 2:35 PM | |
Joined: 6/16/2023 Last visit: 3/4/2025 Posts: 9 Rating:
|
Hi, yes it was the date and time. Wow I would have never found this on my own. Thank you so much for the quick answer |
10/23/2024 3:44 PM | |
Posts: 1 Rating:
|
hi i already tried to modify date and time in both, plc and hmi and im still with the same error 190011, what else can i do? |
10/23/2024 4:34 PM | |
Joined: 3/28/2023 Last visit: 2/26/2025 Posts: 27 Rating:
|
Hi, If you have V17 Update 6 installed, take a look at the following entry: https://support.industry.siemens.com/cs/ww/en/view/109820712 |
Last edited by: Moderator_Lan at: 10/24/2024 07:16:01link optimized |
|
3/1/2025 4:52 PM | |
Joined: 5/13/2024 Last visit: 3/1/2025 Posts: 1 Rating:
|
Here is the solution |
Last edited by: Moderator_Lan at: 03/03/2025 08:31:13Video embedded. |
|
Follow us on